LPC Expresso: Build error for PN7462 CCID Example.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Expresso: Build error for PN7462 CCID Example.

2,547件の閲覧回数
shiv_patil
Contributor II

Hello Community,

I am using LPC Expresso IDE For the development of the PN7462 NFC CCID Example.
I have Successfully Installed & Activated the free edition of the LPC Expresso IDE.
I have Imported the CCID Example as mentioned in the Document.
While building the application I am getting the following error.

/bin/sh: Heap:Default: command not found
/bin/sh: Post: command not found
/bin/sh: Default: command not found
/bin/sh: Stack:Default: command not found
/bin/sh: End: command not found
/bin/sh: Default: command not found
make: *** [PN7462AU_ex_phExCcid.axf] Error 127


Will you please help me to know, how to solve this error?

Regards,
Shiv Patil.

0 件の賞賛
返信
3 返答(返信)

2,537件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,
Did you test with the development board of PN7462 and the LPCXPRESSO version? And there is the same error for MCUXpresso?
Please kindly clarity.
Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 件の賞賛
返信

2,524件の閲覧回数
shiv_patil
Contributor II

Hello @fangfang 
I am able to make a successful test case of the PN7462 CCID example application over the MCU Expresso IDE & the development board.
Also, I am using the same SDK i.e. PN7462AU-FW_v05.22.01_Full.zip for the LPC Expresso IDE.
LPC Expresso IDE Version is 8.2.2

Will you please help me to know why this error is occurring?

Regards,
Shiv Patil.

0 件の賞賛
返信

2,519件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

If your MCUxpresso runs well. Please use MCUxpresso IDE for your application.
Because LPCXPRESSO is no the update version and there is no the better service.
NOTE: MCUXpresso IDE is now recommended for developers using LPC Cortex-M based microcontrollers. This IDE offers a full-featured development environment for both LPC and Kinetis Arm® Cortex®-M based microcontrollers which fully supports LPCOpen and MCUXpresso SDK. For more details of MCUXpresso IDE, please visit http://www.nxp.com/mcuxpresso/ide.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 件の賞賛
返信