Is it ok to switch VDD and PVDD of CLRC663PLUS on/off while TVDD is powered?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it ok to switch VDD and PVDD of CLRC663PLUS on/off while TVDD is powered?

1,157 Views
pekka_leinonen
Contributor I

Hi,

I would like to keep TVDD of CLRC663PLUS powered most of the time, but I would like to switch VDD and PVDD on/off separately from TVDD to save power. Do you see any problems in this?

Is there fore example a risk that current flows from TVDD power rail into those other power rails which are switched off?

I assume that PDOWN pin should be driven low when VDD and PVDD are not powered. So is following condition ok in a low power device:

- PDOWN = 0

- VDD = 0

- PVDD = 0

- TVDD = 3.3V - 4.2V

Br, Pekka

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,016 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pekka,

VDD, PVDD and TVDD are independent from each other. so I could not see any problem in this, but I could not find what the purpose is as well. Would you please clarify? For power saving? and please also note "A hard power-down is enabled with HIGH level on pin PDOWN."

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,016 Views
pekka_leinonen
Contributor I

Hi Kan,

In my system there are two supplies for CLRC663plus. A 3.3v linear regulator for VDD and PVDD and an other 3.3V - 4.2V for TVDD. Both of these supplier are shared also with other modules than CLRC663plus. There are situations (unrelated to CLRC663plus) where some power saving can be achieved by disabling 3.3V regulator although the other supply 3.3V - 4.2V needs to be kept powered.

Br, Pekka

0 Kudos
Reply

1,016 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Thanks for the clarification! 

Have a great day,
Kan

 


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,016 Views
pekka_leinonen
Contributor I

Thanks!

0 Kudos
Reply