Interfacing PNEV7462B with Linux using HSUART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing PNEV7462B with Linux using HSUART

1,467 Views
cibujose
Contributor I

I have a PNEV7462B V2.2 board which I would like to interface using the HSUART to a Ubuntu Linux PC. Is this possible? If so is there a guide on how to do this?

Also, which library can be used to communicate with the NFC interface - is it libnfc-nic? Is there an example application for this?

0 Kudos
Reply
1 Reply

1,404 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please check the following webinar? 

NFC Software Integration II: How to integrate NFC controllers in Linux|NXP 

I believe that you will find the answer to your questions there, as well as the process you asked for. 

Regards, 

Estephania 

0 Kudos
Reply