IFD driver for PN553

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFD driver for PN553

2,206 Views
c_adharumaraj
Contributor I

We are using a PN553 NFC on a snapdragon board running Android Pie. The PN553 is connected to the main controller through I2C.

We are trying to implement a CCID driver for the PN553. We have been able to get communication working between a Windows PC and the CCID driver.

But when we send an APDU to the PN553 we always get a response 0x1C (command not supported). We figure the issue is with our implementation of the IFD driver of the PCSC.

We find no references to any implementations of the iFD driver for PN553 or any compatible NXP devices. It would be great if anyone can share or point us to IFD driver sources for PN553.

Thanks in advance

0 Kudos
Reply
1 Reply

2,116 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Ashwat,

 If you want to use CCID / PCSC to access NFC reader, use PR533 OR PN7462, please!

PN553 doesn't support CCID / PCSC.

Hope above information is helpful for you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply