I downloaded the windows IoT for the Raspberry Pi 2 but in a 4 Gb there is not enough space

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I downloaded the windows IoT for the Raspberry Pi 2 but in a 4 Gb there is not enough space

1,774 次查看
alejandrogutier
Contributor I

compre un kit PN7120 NFC Controller SBC kit OM5577/PN7120S pero baje el sistema operativo OM5577-PN7120S_Win10IoT_demo_v1.0.zip pero al descomprimir ocupa mas memoria que la que recomiendan de 4 GB, pregunta: requiero instalar en una memoria de 8 Gb o hay una version de OS mas pequeña?

0 项奖励
回复
2 回复数

1,629 次查看
alejandrogutier
Contributor I

no i mean downloaded windows 10 from nxp but in a video it says in a 4 Gb memory can put the image but even in a 8gb memoriy there is no enough memory so used a 16 gb memory but when i try to star the RPi2 with W10 sends an error about PNP_DETECTED_FATAL_ERROR so i don't know i to start again installing one more time the SO W10 in the memory

0 项奖励
回复

1,629 次查看
jimmychan
NXP TechSupport
NXP TechSupport

so you can put the image to the SD card and then boot up the board from the SD card.

0 项奖励
回复