I Need NFC Forum NDEF Library for PCSC example & SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I Need NFC Forum NDEF Library for PCSC example & SDK

Jump to solution
2,910 Views
lxnujrhu
Contributor I

I not found NFC Forum NDEF Library for PCSC  example & SDK for windows 7 , 

it not  at NPX Support.

Can you help me? thank you;

我在NPX 中開發資源中,找不到關於 NFC Forum NDEF Library for PCSC 的SDK &範例

是否有人可幫幫我,謝謝。

PS :無格網誌: NFC Forum NDEF Library for Windows 

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,638 Views
Kan_Li
NXP TechSupport
NXP TechSupport

We have NFC reader library including NDEF support for windows,  but you have to request it from the docstore. Please kindly refer to the attachment for details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,639 Views
Kan_Li
NXP TechSupport
NXP TechSupport

We have NFC reader library including NDEF support for windows,  but you have to request it from the docstore. Please kindly refer to the attachment for details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply