How to prevent NFC tag cloning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to prevent NFC tag cloning

6,592 次查看
rockylane
Contributor I

I am in the process of developing a system that detects counterfeit items. The problem is that most NFC tags can be read and duplicated/cloned by individuals who make counterfeit merchandise. Is there a way to use the NFC ICODE DNA tag or any other tag with a password or encryption to prevent it from being cloned? Can the NFC tag be unique to only one item? 

标记 (3)
0 项奖励
回复
3 回复数

5,468 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear  Rocky Lane,

Hope you are doing great, the security features you mention can be accomplished with the ICODE DNA  first I would like to remark that ICODE is compliant with ISO/IEC 15693 as most of our  HF devices that are compliant with ISO 14443. please check the NTAG 413 DNA if you want something on the 14443. the information regarding this two tags are under NDA(Non Disclosure Agreement) this means that all the information should be sent using secured communication channels and just delivered to the  customers with NDA for ICODE DNA I recommend you check the application notes 368111,368010.

if you do not have NDA please contact one of our certified distributors in order to sign one and get the information.

BR

Jonathan

0 项奖励
回复

5,468 次查看
rockylane
Contributor I

Thanks for the response. I am currently using the NTAG413. How would I program the tag to use Secure Unique NFC Message for authentication? 

0 项奖励
回复

5,468 次查看
yangyouyong
Contributor II

Do you got any message about the Secure Unique NFC Message useage?

0 项奖励
回复