I am designing a custom hardware using stm32 and HTRC11001T I have got communications with the HTRC110 working but when I try and send any of the UID Request commands specified in the HITAG S data sheet I no response that looks like any of the coding responses. I have set up my code to receive the anti-collision coding but it isn't picking up anything. I have attached to photos below of my command
yellow - antenna
blue Dout
解決済! 解決策の投稿を見る。
I finally solved the problem by tweaking the electrical side of things - making sure coil - end is at about 140V. also I changed the timings slightly of the command - using cursors and checking data sheet
Hope this helps anyone with the same problem
I finally solved the problem by tweaking the electrical side of things - making sure coil - end is at about 140V. also I changed the timings slightly of the command - using cursors and checking data sheet
Hope this helps anyone with the same problem
Hello @Felix0209
Hope you are doing well.
Could you please confirm that you have followed this App Note: Read/write devices based on the HITAG read/write IC HTRC110 for the design of your reader?
Is your development based on the Control library HTRC110 we provide? Unfortunately, there is no example for HITAG S, but you could use this library as a reference.
Regards,
Eduardo.
Yes I followed that app note and yes i used the library as a reference
Hi,
By any chance, did you manufacture your device based on our HITAG S IC or is it a product from a third-party?
Regards,
Eduardo.
Hi,
Since this is an end product from a third-party, I would recommend you contacting the product manufacturer for further support on this part.
I apologize for the inconvenience this might cause you.
Regards,
Eduardo.