HELP! :( OpenOCD config for P1014

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP! :( OpenOCD config for P1014

2,874 Views
minapa98
Contributor II

Hello, I am currently working on JTAG, I have taken apart a WLAN ACCES POINT and have removed the board. I searched the chip and discovered that my SoC (P1014) has a JTAG interface. I wanted to use OpenOCD for this interface, but unfortunately it doesn't support my chip. My chip is the P1014 from NXP. I was thinking of writing a config for it, but unfortunately it was not that easy for someone with zero experience in that. Does anyone happen to have a config for the P1014 or something similar? Or maybe tips. I would be very happy about everything.


Thank you :smileyhappy:

4 Replies

2,769 Views
yipingwang
NXP TechSupport
NXP TechSupport

OpenOCD didn't support CodeWarrior TAP and P1014.

You could use CodeWarrior for PA 10.5.1, I uploaded CodeWarrior for PA 10.5.1 installation file https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing

2,769 Views
minapa98
Contributor II

Thanks for the quick reply and for the help :smileyhappy:
I need a JTAG debugger for this? or is that somehow also possible with the Raspberry Pi :smileyhappy:

0 Kudos
Reply

2,769 Views
yipingwang
NXP TechSupport
NXP TechSupport

It's not possible with Raspberry Pi.

2,769 Views
minapa98
Contributor II

Thank you for the help!

0 Kudos
Reply