Getting Started PN7462 with raspberry pi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting Started PN7462 with raspberry pi

1,998 Views
shiv_patil
Contributor II

Hello Community,

I am very new to the NFC PN7462 

I would like to interface the PN7462 with the Raspberry Pi board as a host device, which must have the following capabilities.

1. Host must have Reader/Writer Capabilities.

2. Must support all types of interfaces.

3. Need full control on PN7462 using the raspberry pi based application.

 

Will you please help me to know,

1. Which IDE should I use for development? (IAR/MCUXpresso)

2. Is MCUXpresso free for use?

3. Which example is suitable for the PN7462?

4. Software library/SDK for Raspberry Pi environment?

 

Regards,

Shiv Patil.

 

 

0 Kudos
Reply
2 Replies

1,984 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>>1. Which IDE should I use for development? (IAR/MCUXpresso)
Yes, MCUXpresso/IAR is suitable.

>>2. Is MCUXpresso free for use?
Yes, It is free.

>>3. Which example is suitable for the PN7462?
4. Software library/SDK for Raspberry Pi environment?
Please download the NFC library for it.
URL:https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NF....

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

1,975 Views
shiv_patil
Contributor II

Hello, fangfang

Thanks for the reply.

We need a host controller PN7462 Application which communicates with the Raspberry pi to read & write all contactless cards.

There are too many examples in PN7462AU-FW_v05.22.01_Full.zip

Will you please elaborate on your answer.

3. Which example is suitable for the PN7462 for our use case?

 

Regards,

Shiv Patil.

0 Kudos
Reply