Getting 6E00 while using DESFire AES authentication with SAM AV2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting 6E00 while using DESFire AES authentication with SAM AV2

2,324 Views
dev-support
Contributor II

I'm using SAM AV2 for DESFire EV1 personalization. When I'm sending SAM_AuthenticatePICC sequence, I'm getting 6E00 (Class not supported) error from DESFire EV1.
I'm following "AN1826 – MIFARE SAM AV2 – For MIFARE DESFire EV1" and "P5DF081 – MIFARE Secure Access Module SAM AV2".

Logs:
SENT TO PICC: AA00
RECV FROM PICC: AF825287D60A07CC7CA5D9E6A693D60A77
SENT TO SAM: 800A0000120200825287D60A07CC7CA5D9E6A693D60A7700
RECV FROM SAM: B7090E75020F074FEF4C2C2E79DB370F5D026BF43B66CF8253F992E9A194900E90AF
SENT TO PICC: AFB7090E75020F074FEF4C2C2E79DB370F5D026BF43B66CF8253F992E9A194900E
RECV FROM PICC: 6E00

0 Kudos
Reply
2 Replies

2,251 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Tithi Patel,

Hope you are doing great, as you may know the information regarding Mifare SAM and DESFire, is secured under NDA ( Non Disclosure Agreement) which means that all the information, tools and support should be delivered using secured communication channels and only to customers with active NDA.  this is a public forums where we cannot discuss secured information,  my only recommendations here, is that you check that the SAM is in the Mode you are sending the commands, AV1 or AV2 mode,  that the DESFire MK is the type you are using,  and the correct values for the Keys in the SAM and the Keys in the DESFire.

if you keep having issues please let me know if you have any distributor that can help you in a secure communication channel.

Have a great day !

BR

Jonathan

0 Kudos
Reply

2,251 Views
dev-support
Contributor II

The issue has been solved.

0 Kudos
Reply