Hi Tomas,
Thank you very much for the information.
We have since conducted tests by gluing copper tiles (8 mm x 8 mm, spaced 2 mm apart, 2 layers each) to the antenna surface on both the top and bottom.
We then measured the antenna and rematched it.
We can’t detect any differences in terms of functionality (range, current measurement, and EMI).
You wrote that you would recommend a conventional design.
Are there reasons for this, and if so, what are they?
Maybe several smaller areas with more spacing between them would be better than the 8x8 mm with 2 mm spacing?
Thank you very much,
Michael