Clrc663 lpcd interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clrc663 lpcd interrupt

2,005 Views
srini1
Contributor II

Hi I am using clrc663 with stm32l151 spi interface there I want  implement lpcd interrupt mode i don't know the flow I tried but I getting so many irq triggers without card i done calibration I get I and q value I done polling method lpcd enable qmin qmax imin threshold adjustment but something is missing for interrupt mode i don't know the flow kindly help if anyone know about this 

0 Kudos
Reply
6 Replies

1,980 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @srini1

Hope you are doing well.

Please, take a look at the AN11783 CLRC663 plus Low Power Card Detection. This document describes the principle of the LPCD feature offered by CLRC663 plus, including how to use it and how to optimize the related settings.

Also, our recommended NFC Reader Library includes an example project demonstrating LPCD functionality, I believe you could use it as a reference.

Regards,
Eduardo.

0 Kudos
Reply

1,974 Views
srini1
Contributor II
I am using the library provided by NXP there are no major changes in the calibration or any other function in LPCD functions but the IC gives a periodic interupt to the mcu since we are using STM32 as our MCU we cant use the demo code that you have provided. If there are any other library for different MCU can you share it.
0 Kudos
Reply

1,963 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @srini1

As I understand, you are using a custom board based on CLRC663, and not our OM26630FDK, is this correct? If so, could you please confirm that you have followed the Antenna Design Guide for CLRC663 and that you have performed a proper antenna tuning?

You can take a look at the Measurement and tuning of a NFC and Reader IC antenna with a MiniVNA; this Application Note gives a guideline on how to measure and tune/match a NFC and Reader IC antenna with a MiniVNA network analyzer. Also, you can refer to How to use the NanoVNA for the NFC reader antenna design.

Regards,
Eduardo.

0 Kudos
Reply

1,940 Views
srini1
Contributor II
we are using the CLRC66303HNE model ic can you please specific the register and bits that holds the lpcd enable and flag bits
0 Kudos
Reply

1,929 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Our NFC Reader Library supports some compatible Host MCUs from NXP's portfolio, porting this library to any third-party platform is out of our support scope. The only recommendation I could give is to please refer to the following guides: NFC Reader Library Porting FRDM_K64F, Using NFC Reader Library with LPC55S69 and NFC Reader Library Porting to i.MX RT1050 - NXP Community, and make sure to follow a similar process when porting to the MCU used in your setup.

LPCD principle, settings and optimization are described in AN11783 CLRC663 plus Low Power Card Detection. For complementary information, please refer to CLRC663 plus Data Sheet.

Regards,
Eduardo.

0 Kudos
Reply

1,943 Views
srini1
Contributor II
ok we will check antenna but do you guys have any other library file to us with different mcu
0 Kudos
Reply