Card emulation con Raspberry Pi Model A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Card emulation con Raspberry Pi Model A

3,153 Views
alexandredupuis
Contributor I

Hi everybody,

I've installed the card emulation examples on my Raspberry Pi which is a Model A. I have stopped the neard daemon as specified in the docs and started the example with explorenfc-cardemulation -t "Hello NFC".

I have tried to tap my smartphone over the card and nothing happens.

I know card emulation NFC works with my phone because I've used it with another NFC emulation technology.

I'm also quite sure the NXP shield is properly inserted into the GPIO pins of the Raspi, because the tag reading examples work.

Is there anything I've missed?

Best,

Alex

Labels (1)
0 Kudos
Reply
1 Reply

2,801 Views
ToniZollikofer
NXP TechSupport
NXP TechSupport

Hi,

I am not 100% sure if it is required to circle the potential problem, but how about specifying which module you are using? OM5577 with the PN7120 on it?

Toni

0 Kudos
Reply