Capacitor rating for PN5190

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Capacitor rating for PN5190

949 次查看
jr_hernandez
Contributor II

Hi,

I need to confirm the voltage rating for capacitors in matching network for PN5190 EVB (PNEV5190B).

The BOM in the design files is not fully detailed with commercial part numbers so I can not find compatible parts.

I think they are rated to 250V because a collegue could open the source altium file, but I need confirmation asap because we would like to use 0603/0402 instead of 0805.

One question:

Why do matching capacitors in CLEV6630B_V2.0 are rated to 50V and 250V for PNEV5190B if both Front Ends are specified to have 2W?

Please, provide fulll detailed BOM for PNEV5190B base board at your earliest convininence.

Regards, Ramon.

 

 

 

 

0 项奖励
回复
0 回复数