CLRC66303 - Reducing Transmission Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC66303 - Reducing Transmission Power

1,555 Views
stefanmueller
Contributor II

Dear Ladies and Gentlemen,

we are using the CLRC66303 chipset and we want to reduce the transmission power.

We cleared the Cwmax bit and set_cw_amplitude value (TxAmp) to 3 (-1000mV). This does not changed the power consumption of the reader nor does it reduce the output voltage on the Tx1 pin.

Questions:

1. Are our assumption wrong, that set_cw_amplitude should change the transmission amplitude?

2. What is purpose of set_cw_amplitude?

3. Are there any other possibilities of reducing power?

Best Regards

Stefan

0 Kudos
Reply
1 Reply

1,544 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @stefanmueller ,

 

The set_cw_amplitude value (TxAmp) does adjust the transmission amplitude, please see my test result from CLEV6630B board with Cockpit 5.8. The probe takes place right after the EMC filter.

set_cw_amplitude = 0

set_cw_amplitude = 0.png

set_cw_amplitude = 3

set_cw_amplitude = 3.png

 

If the power is still a little bit high, you may try to tune the antenna with a higher impedance.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply