CLRC663 UART read multiple byte in FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 UART read multiple byte in FIFO

1,791 Views
tom19tom
Contributor I

Dear ,

May I know does CLRC663 can read FIFO information more than one byte a time via UART? it seems very slow if my content is more than 50 byte?

Thank you

with regards

David

Tags (1)
0 Kudos
Reply
1 Reply

1,696 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Currently, the examples of the NFC Reader Library are for SPI communication, but you may refer to the following community thread where a recommendation about UART was made: https://community.nxp.com/message/1231077?commentID=1231077#comment-1231077 

Hope it helps!

BR,

Ivan.

0 Kudos
Reply