Bit error count from MFRC531?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bit error count from MFRC531?

1,795 Views
deanfjellerad
Contributor I

Hi

Is there any way I can get bit error count from MFRC531? It is to help me optimize read/write distance.

0 Kudos
Reply
2 Replies

1,688 Views
deanfjellerad
Contributor I

HI Ken

Thanks for reply.

the error reg does not seem to change much.

the closest i could get a error count is to use the s valid signal.

but it also have a very tight tolerance, making it almost useless for that job.

0 Kudos
Reply

1,688 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I am sorry, but MFR531 just supports parity and CRC error detection, do you mean bit collision detection?

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply