I'm testing with IMX6ULL+PN7160_EVK.
At first, the initialization and parameter configuration are normal, But when I send the RF_DISCOVER_CMD to PN7160, there is a lot of clutter on the IRQ pin, and there are some on the IIC pin as well. It is also not possible to check the card properly. When the VBAT_5V is removed, the clutter signal disappears.
I've tried using an external power supply to power VBAT and VDD_UP, but the phenomenon is the same.
Please help check.
Hello @ethan_dang1
Could you share the following information:
1) How to connect PN7160 and IMX6ULL?
2) Please provide demsg log
3) Please provide .dts file
BR
kelly
Hello @ethan_dang1
Could you switch to I2C2? Some sensors mounted on I2C1 may cause interference.
BR
kelly