About - SL3S1003FUD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About - SL3S1003FUD

3,317 Views
412606060
Contributor I

关于这个芯片-SL3S1003FUD,是否可以设计成用继电器短接或断开OUT-VDD,开启或者关闭芯片射频功能?pastedImage_1.png

如果不行的话,请问有哪个型号的RFID芯片可以实现这个功能?在900M频段的。

谢谢各位。

===================================================================

Regarding this chip-SL3S1003FUD, can it be designed to short-circuit or disconnect OUT-VDD with a relay to turn on or off the chip's radio frequency function?

pastedImage_1.png
If not, which model of RFID chip can achieve this function? In the 900M band.

Thank you all.

Tags (2)
3 Replies

3,220 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi 李烨,

这两个引脚不是用来开启或者关闭芯片射频功能的,是用来实现tamper alarm功能的,具体参考下图:

pastedImage_1.png

其他产品好像没有能满足你这个需求的,如果你要实现开启或者关闭芯片射频功能,只能通过连通或断开天线和tag之间的连接来实现。

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,220 Views
412606060
Contributor I

你好,NXP有没有适合做你说的电路的控制芯片,能不能推荐一下,是不是使用射频开关能够实现这个功能?

0 Kudos
Reply

3,220 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi ,

我想你可以看一下UCODE I2C这款芯片,你可以通过单片机连接I2C来控制射频端的开关。

pastedImage_1.png

UCODE I2C | NXP 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply