APDU COMMANDS SAM AV2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APDU COMMANDS SAM AV2

3,315 Views
minhle
Contributor I

I TRY ON  AUTHENTICATING HOST WITH APDU COMMANDS BUT FAULT.CAN YOU SUPPORT FOR APDU COMMANDS SAM AV2?.HOPE YOU CAN HELP ME.

SAM_AuthenticateHost

SAM Command :0x80 0x64 0x0 0x0 0x0

SAM Response :0x0 0x0 0x0 0x0 0x0 0x0 0x0 0x0 0x0 0xff 0x0 0x0 0x90 0x0

SAM Command :0x80 0xa4 0x0 0x0 0x2 0x0 0x0 0x0

SAM Response :0x36 0x67 0x46 0xfa 0x4c 0xba 0x3d 0xdc 0x90 0xaf

SAM Command :0x80 0xa4 0x0 0x0 0x10 0x21 0xa1 0xfd 0x1a 0xa4 0xdb 0xd3 0xdf 0xfa 0x1f 0x8a 0xa 0x50 0x73 0x43 0x75 0x0

SAM Response : 0x90 0x1E

Labels (1)
0 Kudos
Reply
1 Reply

2,215 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello minh le,

Detailed information on SAM AV2 is under NDA, so for support you need to ask your NXP local contact or Sales Representative.

Sorry for the inconvenience and thank you for your understanding.

Regards!

Jorge Gonzalez

0 Kudos
Reply