我们的CPU 是MTK6737,想在Android系统上实现NFC 和PSAM功能,本来想使用PN 7462实现功能,但是新手一枚,在没有资料的情况下没有完成,现在想寻求一种方案,实现这个功能
请问你们做的是什么设备?POS?
是的。我在做POS。在MTK平台上,Android版本为6.0
13102370205@163.com
发件人: Kan_Li
发送时间: 2017-05-09 11:16
收件人: 小雨 李
主题: Re: - Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能
NXP Community
Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能
reply from Kan_Li in NFC - View the full discussion
请问你们做的是什么设备?POS?
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in NFC by email or at NXP Community
Following Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能 in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
如果是Android POS一般都会另外再挂一个不跑系统或者跑实时操作系统的安全MCU再接非接和接触式模块, 你可以使用K21/K81/i.Max + RC663的方案。
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------