使用PN7150多次读取Tag之后出现异常

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

使用PN7150多次读取Tag之后出现异常

2,766件の閲覧回数
466231674
Contributor I
android7.1平台,使用的PN7150型号的NFC,在read tag测试的时候,有概率会引起NFC工作异常(多次read tag之后,read无响应),在出现异常之后,只能通过设置关闭重新打开才能使NFC正常工作。附件是测试的logcat日志,初步对日志做了分析,在出现如下log之后NFC就不能正常工作了
 09:06:06.724 I/BrcmNfcNfa( 4526): NFA got event 0x0600
 09:06:06.724 I/BrcmNfcNfa( 4526): nfa_rw_handle_event event: NFA_RW_OP_REQUEST_EVT (0x600), flags: 00000001
   09:06:06.724 E/BrcmNfcNfa( 4526): nfa_rw_handle_op_req: not activated
タグ(1)
0 件の賞賛
返信
7 返答(返信)

2,159件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

have you try to add 'printk' to check where it stop?

0 件の賞賛
返信

2,159件の閲覧回数
466231674
Contributor I

hi Jimmy:
I find this log comes up every time(E/BrcmNfcNfa(?4526):?nfa_rw_handle_op_req:?not?activated),After that, the NFC cannot work

0 件の賞賛
返信

2,159件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Hi Zhonggan,

Nice to talk to you on the phone. You mentioned you have tested on different App. Could you tell me your test steps and which App you used in the test?

Thanks.

0 件の賞賛
返信

2,159件の閲覧回数
466231674
Contributor I

hi Jimmy:
You can check the video for the test steps,The video was tested using the apk of the NFC TagWriter,And you can see that from video,The testing process is to use Tag intermittently close to the NFC antenna,When apk detects Tag, it will respond,At the same time, we can hear the response(voice),In the second half of video,We can see that the NFC is no longer responding,We can't hear the response(voice) as normal,That's what I call the anomaly。
When the apk was tested using the NFC TagInfo,That's not going to happen。Can you give me your email address? I can send the test video to you。tks!

0 件の賞賛
返信

2,159件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,159件の閲覧回数
466231674
Contributor I

hi Jimmy,pls check email,tks。

0 件の賞賛
返信

2,159件の閲覧回数
466231674
Contributor I

hi Jimmy:

  I used two apk tests, NFC TagWriter.apk and NFC TagInfo.apk

I uploaded two apk to the attachment

0 件の賞賛
返信