For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?

1,101 Views
greg_turner
Contributor I

For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?  Trying to implement additional card type support on existing code.

Labels (1)
0 Kudos
Reply
1 Reply

962 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

As I know, 0x00, 0xA4 is "Select File" command.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply