--The document consists of the following:
Step 1. Connections And Firmware Version
Step 2. Updating FW On PC Windows 10
Step 3. Updating FW On VMplayer16.0 + Ubuntu 20.04
Step 4. Updating FW On i.MX8MN-EVK With Embedded L5.4.70_2.3.0 BSP
Step 5. Confirming whether update is successful using cockpit4.8
--About Cockpit
There are several different versions of cockpit, and each version can only recognize the same version of firmware.
--Reference Materials
1.https://community.nxp.com/t5/NFC/Mounting-the-PN7462AU-in-the-USB-downloader-mode-under-Linux/m-p/80...
2.https://community.nxp.com/t5/NFC/PN7462-updating-EEPROM-on-linux/m-p/739808/highlight/true#M3144
NXP CAS-TIC team
Weidong Sun
04-15-2021