Which IDE to use for ACIM FOC project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which IDE to use for ACIM FOC project?

3,032 Views
RamFa
Contributor I

Hi,

We've purchased the HVP-MC3PH platform and successfully got the accompanying FW compiled in KDS and downloaded and run on HVP-KV46F150M board. My question is now this: considering that the KDS IDE seems to be obsolete, what do you recommend,  port  to MCUXpresso or continue with KDS? And if the former alternative is recommended is there any guide to help?

Thanks/ Ramin

 

0 Kudos
Reply
2 Replies

3,008 Views
RamFa
Contributor I

Thanks, We give it a try and get back in case of trouble.

Regards/Ramin

0 Kudos
Reply

3,020 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ramin,

We recommend switching to MCUXpresso. There is an SDK available for the HVP-KV46F150M.

There is not an automatic tool to convert the project from KDS to MCUXpresso, so you would need to create a new project for your board from MCUXpresso and then importing your sources and work on necessary changes from there.

The following Knowledge Base document provides additional information.

https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/Moving-to-MCUXpresso-IDE-from-Kinetis-Des...

I hope that this information helps!


Regards,
Gustavo

0 Kudos
Reply