Re: How to use freemaster to debug a new motor,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: How to use freemaster to debug a new motor,

1,085 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

FreeMASTER cannot help you to debug a motor. It is a tool which shows you variable values of your example application and can modify them to do some control over the application behavior. The graphical interface enables to host interactive Dashboards and other Control pages which can do the same thing (read/write variables) using a custom user interface.

One of the "custom" interfaces provided by NXP Motor Control team is the MCAT - Motor Control Application Toolbox, which you can use to debug motor control example applications of the NXP MCUXpresso SDK packages.

Please try describing your hardware and the problem you have (microcontroller, motor type, SDK example). I'm moving this thread to Motor Control and Smart Energy community.

Thanks,
Michal

 

0 Kudos
Reply
2 Replies

1,095 Views
zhouqicheng
Contributor I

How to use freemaster to debug a new motor, which parameters need to be changed, and do you have a manual

0 Kudos
Reply

1,080 Views
MichalH
NXP Apps Support
NXP Apps Support

Please see my reply on at the top of this thread. The community has reversed an order of the messages when moving it from the FreeMASTER forum.

Regards,
Michal

0 Kudos
Reply