Piezoelectric Actuator transducer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Piezoelectric Actuator transducer

520件の閲覧回数
cmfseo
Contributor I

Piezoelectric Actuator Transducers are devices that leverage the piezoelectric effect to convert mechanical stress into an electric charge or vice versa. Here's a detailed explanation based on the provided search results:

Definition
A piezoelectric transducer is a device that uses the piezoelectric effect to measure changes in acceleration, pressure, strain, temperature, or force by converting this energy into an electrical charge. It can also function as an actuator, where the electric effect causes the material to deform, either stretching or bending when voltage is applied.

Working Principle
The working principle of a piezoelectric transducer is based on the piezoelectric effect, which allows these transducers to generate voltage when mechanical stress is applied. This effect is reversible, meaning that applying an electric potential across a piezoelectric material can cause it to change shape or size.

Material Properties
Piezoelectric materials, such as quartz crystal (SiO2), are essential for the transducer's function. These materials respond uniquely to mechanical stresses and generate electrical polarity under mechanical stress, which can be either compressive or tensile.

Piezoelectric actuators and transducers are highly valued for their precision, sensitivity, and versatility in various sensing and actuation applications across different industries.

0 件の賞賛
返信
0 返答(返信)