PMSM vs BLDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMSM vs BLDC

3,371 Views
abderrahimjamao
Contributor III

Hello,

can I use two different algorithms (FOC and SIX-step) to drive my brushless motor? So, I mean, is there a difference when I use the FOC control or the six-step control for the same engine.

4 Replies

3,280 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

can I use two different algorithms (FOC and SIX-step) to drive my brushless motor?

Yes , you can.

So, I mean, is there a difference when I use the FOC control or the six-step control for the same engine.

yes, there is difference.

FOC is constant 90 degree magnetic angle drive, which provides best efficiency

Efficiency comparison between six step and FOC for a given motor - Electrical Engineering Stack Exch... 

regards,

Peter

3,280 Views
abderrahimjamao
Contributor III

Good morning,

Thank you.

I am trying to control my brushless motor (Gear hub motor) by the MTRDEVKSPNK144 project. It is therefore blocked in the calibrated state then goes to the fault state and indicates that the fault comes from the current Ia.iaa.PNG

0 Kudos
Reply

3,280 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

First would be nice to know what kind of motor do you have (parameters).

You need to find why you have overcurrent.

I don't think this is caused in calibration mode, rather in align state.

The first guess would be:

Small resistance of motor. In this case the 1V for align can cause overcurrent.

regards,

Peter

 

3,280 Views
abderrahimjamao
Contributor III

Yes, you are right, I corrected it when I make the AlignVoltage at 0v.

0 Kudos
Reply