BLDC motor controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC motor controller

3,901 Views
Tarun99
Contributor I

I'm looking for Bldc motor controller for 2kw bldc motor, operating voltage 48v/60v with 2800 RPM 3 phase. I'm using Nvidia jetson nano processor. Please suggest me some controller which can easily communicate with processor.

 

0 Kudos
Reply
3 Replies

3,088 Views
Boured
Contributor I

Are BLDC motors better than brushed DC motors?

0 Kudos
Reply

3,763 Views
stevediaz
Contributor I

For a 2kW BLDC motor with a 48V/60V operating voltage and 2800 RPM, consider motor controllers like Roboteq HDC2450, ODrive, VESC, Trinamic TMC4671, or TwinCAT 3 with EtherCAT support for communication with your Nvidia Jetson Nano. Ensure compatibility with your motor's specs and your Jetson's communication interfaces.

0 Kudos
Reply

3,855 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

The output power of our High-Voltage Development Platform support up to 1 kW. On the other hand, MCSXTE2BK142 supports up to 800W.

In general our reference design boards are for low power. So the customer would have to develop their own power stage. For this you can use our 3-Phase Brushless Motor Pre-Driver and propose your own 3-ph bridge.

You can also refer to our example projects for motor control MCUXpresso SDK for Motor Control and Automotive Motor Control Solutions.

Hope it helps you.

Have a nice day!

0 Kudos
Reply