s32k144 pmsm closed loop mbd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 pmsm closed loop mbd

854 Views
Sriram
Contributor IV

Hello,

I am trying to modify the pmsm closed loop model and run a 120v pmsm  with a sine encoder which gives me absolute value of the rotor position. The motor is aligning and then going into forced mode and running fine but once it goes into tracking mode it stops spinning. 

I want to know what happens during the alignment phase and why the offset is taken as either 90 or -90 degrees and the subsequent operation in the tracking mode and the transition from tracking mode to sensored mode.

my motor has 5 pole pairs

1.png1.png

Thank you

Tags (1)
0 Kudos
Reply
0 Replies