problem with PIL simulation on NXPs32k144 evb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with PIL simulation on NXPs32k144 evb

2,142件の閲覧回数
pierpaolo_dini
Contributor III

I encountering issues with concretize PIL procedure.

I face the following error in simulink

 

Cannot perform PIL simulation for "Esempio_0". Configuration parameters for this model do not support these connectivity configurations: IBIS_AMI, Arduino Board, Texas Instruments Code Composer Studio (IDE), Texas Instruments Code Composer Studio (TCP/IP), Texas Instruments Code Composer Studio (Serial), s32k_pil PIL, s32k_as_pil PIL Update configuration parameters or create a supported connectivity configuration. For more information, see Help Center.

 

i am sure that all the setup oprions are right (solver, settings i configure the HW implementation, th target block is right...), but i dont know why i face this error.

 

Its strange that if i build the code through the embedded coder app i face no problems in flashing the evb.

With harnest and SIL/PIL test apps instead i have such issue.

 

Can some one help me?

 

Thanks in advance

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,107件の閲覧回数
pierpaolo_dini
Contributor III

No one from technical support of NXP is able to provide solution or at least suggestion for workaround??!!

0 件の賞賛
返信

2,077件の閲覧回数
pierpaolo_dini
Contributor III

@paulvlase 

i remember you help me with another issue, so i invoke you.

Can you suggest something to do?

Thanks in advance.

0 件の賞賛
返信