gpio_s32k14_output block (mask) does not have a parameter named 'port'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpio_s32k14_output block (mask) does not have a parameter named 'port'

2,436 Views
1586526941
Contributor I

gpio_s32k14_output block (mask) does not have a parameter named 'port',How to solve this problem?

0 Kudos
Reply
2 Replies

2,360 Views
constantinrazva
NXP Employee
NXP Employee

Hello 1586526941@qq.com‌,

Can you provide the example you are trying to build?

A few more questions to get a better understanding of the context - do you have the correct path set ? Do you have multiple toolboxes installed ? Maybe more versions of the S32K toolbox?

Can you send me the output of the following MATLAB command:

ver

Kind regards,

Razvan.

0 Kudos
Reply

2,360 Views
1586526941
Contributor I

hi

    the toolbox version is MBDToolbox S32K1xx_2018.R1_20180723.mltbx,when the Dightal_Output is existing,to load the Write_Register, this problem will arise.

0 Kudos
Reply