ert_rtw

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ert_rtw

1,505 Views
paul_ephraim_13
Contributor III

Good Morning Sir/Madam,

I have been working with the nxp mbdt toolbox in Simulink. Every time I create a PWM or adc or Dio model, Only the initial configuration settings are updated in the target (s32k312). If I bring about a change in the model, Even after building the model to the target the processor seems to function with the initial build. I have posted this query before and tried the suggestion received from the nxp community: to check with the Port Component Configuration and delete the ert file generated. However, although the port component configuration was all done, I still had the issue. I tried deleting the ert file and it seems to solve the issue, but I have to do the deletion before every build process to the target. Kindly clarify the issue. I have attached the  simulink file.  I have also uploaded the images. 

 

From the first image, I have the set led to blue and built the model into the target. The second image verifies that with the generated c code. However, with the third image, I changed the parameters to green from blue and that is also reflected in the code. However, the second time I built the model the change is not effective in the target. It only becomes effective, only when I manually delete the ert_rtw file every time . Kindly clarify the issue. first image where led is bluefirst image where led is blueblue led generated codeblue led generated codeblue to green led code(changed)blue to green led code(changed)

Labels (1)
0 Kudos
Reply
0 Replies