devkit MPC5744P communication test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

devkit MPC5744P communication test

Jump to solution
4,639 Views
henryex2009
Contributor I

 Hi everyone,

 I used MPC5744P to test UART . I successfully download the "Hello word" example to the DEVKIT 5744P

through this MBT tool(Version 3.2),but the Tera Term show nothing. Please tell me how to solve this problem.

BTW, the CAN commuication example also has same problem.The model is download into DEVKIT 5744P,but I can't see the CAN RX/TX( by INCA).

0 Kudos
Reply
1 Solution
4,553 Views
hbhnhbnhj1
Contributor III

Hi @henryex2009,

You can change the serial port to 0 as shown in figure below, it should work.

hbhnhbnhj1_0-1650447710662.pnghbhnhbnhj1_0-1650447710662.png

 

View solution in original post

0 Kudos
Reply
3 Replies
4,554 Views
hbhnhbnhj1
Contributor III

Hi @henryex2009,

You can change the serial port to 0 as shown in figure below, it should work.

hbhnhbnhj1_0-1650447710662.pnghbhnhbnhj1_0-1650447710662.png

 

0 Kudos
Reply
4,513 Views
henryex2009
Contributor I

Hi,hbhnhbnhj1,

It works,thank you for your assistance

0 Kudos
Reply
4,506 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @henryex2009

Please have a look at the Schematics of the EVBs before developing your application, to make sure that the right pins are selected inside the blocks, alongside the right UART instances.

https://www.nxp.com/design/development-boards/automotive-development-platforms/mpc57xx-mcu-platforms... 

Hope this helps,

Marius

0 Kudos
Reply