channel id error for dio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

channel id error for dio

Jump to solution
398 Views
Vijay98
Contributor II

Hello nxp team,

we are trying to enable the PTD17 pin high with dio peripheral

port name: PTD_H

Dio port Id: 7

Dio channel Id: 1

how to check the channel id i set is correct or not?

right now this pin is not getting high.

Labels (1)
0 Kudos
Reply
1 Solution
329 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vijay98 

For achieving a correct configuration of PTD17 inside the Dio component, could you please check the following article (link)? It provides a complete description of the mapping between the Port Id, Channel Id and the pin that should be configured.

The article also presents a demo application, showcasing how certain values can be written to the pins, or how the pins values can be read, using the APIs exposed by the MBDT Dio Simulink block.

Hope this helps,

Irina

View solution in original post

0 Kudos
Reply
1 Reply
330 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vijay98 

For achieving a correct configuration of PTD17 inside the Dio component, could you please check the following article (link)? It provides a complete description of the mapping between the Port Id, Channel Id and the pin that should be configured.

The article also presents a demo application, showcasing how certain values can be written to the pins, or how the pins values can be read, using the APIs exposed by the MBDT Dio Simulink block.

Hope this helps,

Irina

0 Kudos
Reply