Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

6,403 次查看
littlepirate
Contributor I

Hi,

   I can use the CAN_Receive_Data_Trigger module in model-based Design Toolbox for MPC57xx, version 2.0.0, but I cannot use it in version 3.0.0.

   With this Error: simulink. DataType object 'status_t' is not in scope from 'untitled/FCAN_Receive'.

   Is there any good solution?

   Thank you very much!

0 项奖励
回复
5 回复数

6,149 次查看
dea
Contributor I

Hello! I have the same problem. How did you solve this problem?

0 项奖励
回复

6,149 次查看
chenli2
Contributor II

No solution. No answer from NXP.

Sent from Ding Mail

0 项奖励
回复

6,149 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello 欣澍 杨,

The toolboxes 3.0.0 and 2.0.0 are not compatible between them, so please do not use blocks from the 2.0.0 in 3.0.0 or reverse. The MPC57xx 3.0.0 is based on S32 SDK for Power Architecture so more or less the output for some blocks are now provided from others. We also do provide examples for CAN so please have a look on them before.

Hope this helps,

Marius

0 项奖励
回复

6,091 次查看
j_wale_3
Contributor II

It seems this still has not been fixed in MBDToolbox version 3.2.0. Any comment from NXP, please? It's preventing commercial work in my case.

Thanks,

John.

0 项奖励
回复

6,149 次查看
chenli2
Contributor II

Hello,

There is NO example of CAN receive for Blocking mode. All example are non-blocking mode.  I am using Version 3.0. When I change the mode, I got error message "Simulink.DataType object 'status_t' is not in scope from 'SoftwarePlatformMPC5744/Subsystem7/CAN/CAN 0 Rx/FCAN_Receive1'.

Can you show me an example of blocking mode CAN receiver?

Li