Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

6,410 Views
littlepirate
Contributor I

Hi,

   I can use the CAN_Receive_Data_Trigger module in model-based Design Toolbox for MPC57xx, version 2.0.0, but I cannot use it in version 3.0.0.

   With this Error: simulink. DataType object 'status_t' is not in scope from 'untitled/FCAN_Receive'.

   Is there any good solution?

   Thank you very much!

0 Kudos
Reply
5 Replies

6,156 Views
dea
Contributor I

Hello! I have the same problem. How did you solve this problem?

0 Kudos
Reply

6,156 Views
chenli2
Contributor II

No solution. No answer from NXP.

Sent from Ding Mail

0 Kudos
Reply

6,156 Views
mariuslucianand
NXP Employee
NXP Employee

Hello 欣澍 杨,

The toolboxes 3.0.0 and 2.0.0 are not compatible between them, so please do not use blocks from the 2.0.0 in 3.0.0 or reverse. The MPC57xx 3.0.0 is based on S32 SDK for Power Architecture so more or less the output for some blocks are now provided from others. We also do provide examples for CAN so please have a look on them before.

Hope this helps,

Marius

0 Kudos
Reply

6,098 Views
j_wale_3
Contributor II

It seems this still has not been fixed in MBDToolbox version 3.2.0. Any comment from NXP, please? It's preventing commercial work in my case.

Thanks,

John.

0 Kudos
Reply

6,156 Views
chenli2
Contributor II

Hello,

There is NO example of CAN receive for Blocking mode. All example are non-blocking mode.  I am using Version 3.0. When I change the mode, I got error message "Simulink.DataType object 'status_t' is not in scope from 'SoftwarePlatformMPC5744/Subsystem7/CAN/CAN 0 Rx/FCAN_Receive1'.

Can you show me an example of blocking mode CAN receiver?

Li