Hi Hj,
From your error file it looks like your MATLAB installation is in a path with " " _spaces and that seems to trigger the error.
sim_sil_target.mk:173: E:/Program: No such file or directory
sim_sil_target.mk:173: Files: No such file or directory
sim_sil_target.mk:173: (x86)/MATLAB/R2013b\rtw\c\tools\lcctools.mak: No such file or directory
gmake: *** No rule to make target `(x86)/MATLAB/R2013b\rtw\c\tools\lcctools.mak'
What i suggest is to:
- reinstall MATLAB in a path without spaces: e.g. C:\MATLAB
- use Microsoft Software Development Kit (SDK) 7.1 to get the compiler: Download Microsoft Windows SDK for Windows 7 and .NET Framework 4 from Official Microsoft Download C...
With this setup it should work flawless:
My setup: Win7 + Matlab2013b + MSDK7.1
Hope it helps!
Daniel
Hi Daniel,
Though reinstalling MATLAB in a path without spaces and using Microsoft Software Development Kit (SDK) 7.1 ,I still fail to compile the MPC5643L toolbox examples and it always hints that .mexw32 file does not exist.With the same method ,the problem never occur in other computer,only exsiting in mine.So what happens in my computer?Can you give me some suggestions?
Thanks a lot.
Hj
Hj,
I'm sorry for this situation. Let's go back to basics. Can you compile any C-source file with your Matlab setup ?
Please compile the file attached: in Matlab command line run:
>> mex main.c
Building with 'Microsoft Windows SDK 7.1 (C)'.
MEX completed successfully.
Does it creates a main.mexw64 or main.mexw32 file ?
Best regards,
Daniel
You still have issues with the paths. Inside the toolbox there is a directory that contains spaces "MCLIB for MPC564xL". Your Windows operation system does not handles the paths correctly and the Matlab looks for the path until the first space (wrong) and that is why it complains and fails.
To confirm this, please open a command line (cmd.exe) on your computer and run this command:
FSUTIL.EXE 8dot3name query E:
Paste here (in english) the return results.
Hi Hj,
Personally i do not know other way. You should ask your system administrator to handle this since it appears your user does not have administrative privileges.
I believe your computer is not configure to handle paths that contains spaces and/or are too long (8.3 filename - Wikipedia)
Best regards,
Daniel
Hi Daniel,
After running the command ,the hints are as follows
C:\Users\Administrator>FSUTIL.EXE 8dot3name query E:
volume state is: 1 (8dot3 name is forbidden to be built)。
registry state is : 2 (Set by volume - defaults)。
base on the configuration above,8dot3 name is forbidden to be built on E
Can you give me some suggestions?
Thanks a lot.
Hj
Hi Hj,
This explains why on your computer the long path that contains spaces are break into multiple commands that are not recognized. Here are my settings. You can also check this command on the other computers that we said are working.
C:\Users\b21307>FSUTIL.EXE 8dot3name query C:
The volume state for Disable8dot3 is 0 (8dot3 name creation is enabled).
The registry state of NtfsDisable8dot3NameCreation is 2, the default (Volume level setting).
Based on the above two settings, 8dot3 name creation is enabled on C:.
Ideally would be to try to configure this computer and enable the 8dot3 on E partition.
Hope this helps you to fix the issue.
Best regards,
Daniel
Hi Daniel,
Firstly,I configured this computer and enabled the 8dot3 on E partition as follow.But it didn't heip.Is it the rightway to configure it ?
What's more,I want to know the way to use MCToolbox when MPC5643L working on DPM mode.
Thanks a lot.
Hj