Single shunt current sensing using MBDT / S12ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single shunt current sensing using MBDT / S12ZVM

3,049 Views
Stefan_9811
Contributor II

Hi everybody,

I purchased the S12ZVM High Current Evaluation Board (MCSXSR1CS12ZVM) and want to develop a sensorless FOC using the model based desing toolbox (MBDT).

In the MBDT Library for S12ZVM an FOC example is provided, which uses a dual shunt current measurement. As the MCSXSR1CS12ZVM board has just a single shunt resistor available I am seeking for some example, how to implement a single shunt current measurement for the board with MBDT.

I would really appreciate your help.

Kind regards,

Stefan

0 Kudos
Reply
2 Replies

3,021 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

AN5327

Best regards,

Ladislav

0 Kudos
Reply

3,009 Views
Stefan_9811
Contributor II

Hi Ladislav,

thank you very much for your reply and the documents.

I see that you send me a Code Warrior project in C. Is it also possible to get a Simulink model, which implements the singel shunt current sensing on the "MCSXSR1CS12ZVM" Board? 

Kind regards,

Stefan

0 Kudos
Reply