SPI extra clock pulse generation issue in MBDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI extra clock pulse generation issue in MBDT

399 Views
Vijay98
Contributor II

Hello NXP team,

Currently we are working on SPI communication in MBDT Version 1.5.

And we are facing one issue: that we are getting one extra pulse in the serial clock pin before chip select goes low.

Vijay98_0-1750502016170.jpeg

We can not able to decode this issue.

With this, we are facing challenges in reading SPI commands fro another ic.

I have added the configuration photos which we done.

Vijay98_1-1750502610150.pngVijay98_2-1750502652455.pngVijay98_3-1750502670527.pngVijay98_4-1750502686354.pngVijay98_5-1750502705125.png

 

Kindly help us to resolve this issue ASAP.

@PetrS 

@stefanvlad 

@Irina_Costachescu 

Thanks & Regards,

Vijay

 

0 Kudos
Reply
1 Reply

337 Views
brian159james
Contributor I

Hello,

The extra pulse on the SPI clock line before CS goes low is likely due to incorrect initialization order or pin configuration. Ensure:

CS goes LOW before SPI starts.

CPOL/CPHA match slave requirements.

Avoid SCK glitches by configuring SPI before assigning pins.

Use software-controlled CS with proper sequencing in Simulink.

 

Best Regard,

Brian

0 Kudos
Reply