SPI Initializes four chip select pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Initializes four chip select pins

ソリューションへジャンプ
2,831件の閲覧回数
fernando_barrio
Contributor III

Hi,

I am working with SPI on the S32K, is there any way that I don't have to initialize all four chip select pins? I want three instances of SPI communication each with only one slave/master, but now I have a lot of pins that I cannot use. Please let me know if you have any suggestions.

Thank you,

Fernando

1 解決策
2,687件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

元の投稿で解決策を見る

4 返答(返信)
2,687件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

In the current version of the toolbox there is no such option, but I will post on the Hotfixes page next week an update so you can do just that - it will be there probably Tuesday; I'll post here a link to it as it is made available.

Kind regards,

Razvan.

2,687件の閲覧回数
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

That sounds great, thank you for the support.

Fernando

0 件の賞賛
返信
2,688件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

2,687件の閲覧回数
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

Looks great, I really appreciate the help.

Thank you,

Fernando

0 件の賞賛
返信