S32K344 Low Power Mode Implementation Using MBDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 Low Power Mode Implementation Using MBDT

1,309 Views
chaudharimohit73
Contributor II

Hello,

I am working on the S32K344 MCU using MATLAB/Simulink Model-Based Design Tool (MBDT) and need guidance on implementing Low Power Modes.

I am unable to find a clear, end-to-end procedure for:

  • Configuring low power modes (RUN/STOP/STANDBY or equivalent) using MBDT
  • Required settings in S32 Configuration Tool (PMC, MC_ME, clocks, wake-up sources)
  • Triggering power mode transitions from Simulink/Stateflow
  • Proper wake-up source handling in an MBDT-based project

If there are any reference examples, application notes, or recommended workflows for S32K344 + MBDT low power management, please share.

Thank you for your support.

0 Kudos
Reply
1 Reply

1,224 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

I've created an article that shows how to put S32K344 into standby mode using Model Based Design Toolbox for S32K3 v1.8.0.  Please check How to: Standby mode on S32K3 using NXP MBDT for more information. Moreover, I've attached an example model that you can try. You might have to modify the pin used to wakeup the board and the pin used by the LED.

if you need other ways to wake up the board, you can also check the following article: S32K3 Low Power Management AN and demos .

 

Best regards,

Sorin Bancila