S32K144EVB simulink - LIN Communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB simulink - LIN Communication

721 Views
deepan1994
Contributor I

Hello,

I would like to understand the generic process of implementing a LIN stack in simulink

for example, I have multiple schedule tables with different cycle times, eg 10ms, 20ms, 50ms, 100ms, 1000ms etc..

How do I define these schedule tables in simulink?

What blocks do i need to use for populating the data for signals in the schedule table?

How do I capture the response signal on the schedule table?

I think I can make use of general task scheduling feature of the MBDT , but how do i define in the appropriate task subsystems which are related to LIN communication?

0 Kudos
Reply
0 Replies