S32K - Online Calibration - INCA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K - Online Calibration - INCA

1,932 Views
Sam_ECU
Contributor V

Hello,

We've run into limitations with Freemaster (communication errors due to size and speed of the application).

As a result, we'd like to move over to the industry standard for engine calibration, INCA.

On the ETAS website they offer ETK-Support for the S32K.

https://www.etas.com/en/products/etk_fetk_xetk_ecu_interfaces-supported_microcontrollers.php

Is the S32K capable of supporting the "Working Page / Reference Page" in INCA (and online calibration on the Working Page".

We believe so, as there's an "External Mode" example in MBDT where a constant can be changed live.

How does it work with the S32K?

Is it linked to this issue below?

https://community.nxp.com/t5/S32K/S32K144-How-to-remap-Flash-address-to-Ram/td-p/945566

 

Thanks.

 

0 Kudos
Reply
0 Replies