Run Time Error vs. Freemaster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run Time Error vs. Freemaster

1,171件の閲覧回数
Sam_ECU
Contributor V

Hello,

Is there a way to determine, whether an issue is a run time error due to the code or whether the issue is due to the connection to Freemaster or Freemaster settings?

My model after certain changes (extremely minor) will stop working after a certain period of time in Freemaster, but LED's continue to toggle and an oscilloscope shows that the board is still operating and timers are as expected.

An improvement was found by adjusting the Step Tick Priority and Polling Method for Freemaster, but the issues can still be generated.

 

Is there a method to debug with Freemaster?  Or is debugging in Freemaster, that the connection to the board is lost ([ERROR code=0x80000101]).

 

Thanks for the help.

0 件の賞賛
返信
0 返答(返信)