Reset led toggling while deploying the project from mbdt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset led toggling while deploying the project from mbdt

Jump to solution
1,982 Views
Vijay98
Contributor II

Hello NXP team,

We are working in dio configuration using mbdt with S32K344 EVB Rev B1.

while deploying the code using matlab we are able to see the functionality working but after some time like 3 to 5 sec the board reset LED starts blinking continuously.

Unable to find the solution. Can anyone give me some solutions!

Attached the project folder with this, kindly do some needful.

 

Thanks & Regards

Esakki

 

MBDT @VaneB @Irina_Costachescu @Robin_Shen @Ganapathi_NASH_INDIA @Kavin_raj_mbd 

1 Solution
1,894 Views
dragostoma
NXP Employee
NXP Employee

Hi, @Vijay98,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

Let us know if your problem persists.

 

Best regards,

Dragos

View solution in original post

0 Kudos
Reply
2 Replies
1,895 Views
dragostoma
NXP Employee
NXP Employee

Hi, @Vijay98,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

Let us know if your problem persists.

 

Best regards,

Dragos

0 Kudos
Reply
1,969 Views
Kavin_raj_mbd
Contributor II

Hi esakki,

 

I am also facing the same issue...

In s32k344 evb rev A it's working fine but in s32k344 evb rev B1 after flashing for 5 to 10 sec it's working fine after that reset led starts blinking continuously 

If you find any solution kindly let me know... then any one resolved this issue let us know

 

Thanks & Regards 

KR

 

MBDT S32K3X4EVB-T172 

@VaneB @Irina_Costachescu @Robin_Shen 

0 Kudos
Reply