Hi Kent,
It is relatively simple. First you need to create a New S32DS Project for the MCP5744P.
Then, once the project is created, you will use a trick:
1: go to Debug Configuration
2: select the Flash launch configuration
3. change the project elf to the rbf file you wish to program on flash
4. click on Debug and that will flash the rbf into the MPC
Hope this helps!
Daniel
Hi Kent,
Just to clarify your question:
- do you want to know how to program/write an ELF file using S32DS for Power Architecture existing UI for flash programming?
or
- do you want to implement a flash programming algorithm using S32DS for PA ?
Best regards,
Daniel
Hi Kent,
It is relatively simple. First you need to create a New S32DS Project for the MCP5744P.
Then, once the project is created, you will use a trick:
1: go to Debug Configuration
2: select the Flash launch configuration
3. change the project elf to the rbf file you wish to program on flash
4. click on Debug and that will flash the rbf into the MPC
Hope this helps!
Daniel
Hi Kent,
The MPC5744P is supported by the RAppid bootloader. Before using this tool you need to write MPC5744P.rbf to the target (see ${InstallDir}\mctbx_pnt\tools\BootLoader\RBF_Files\MPC5744P.rbf). You can use "S32 Design Studio for Power Architecture" to perform the flash write. After you need to reset the board and try to use the bootloader directly.
Regards,
Radu
Hi Kent,
You have to define the appKey and other symbols, please see below an example but you can also generate the code as reference, BAM option enable, using the Toolbox and look how the BAM is used. For more details please see "RAppidBL_UserManual.pdf".
C
#pragma section R ".appDelay" ".uappDelay" data_mode=far_abs
__declspec(section ".appDelay") const uint32_t appDelay = 5000000;
#pragma section R ".appKey" ".uappKey" data_mode=far_abs
__declspec(section ".appKey") const uint32_t appKey = 0x55AA55AA;
#pragma section R ".appKeyAddr" ".uappKeyAddr" data_mode=far_abs
lcf
GROUP :
{
.rcw LOAD(0x00FA0000): {}
.appDelay LOAD(0x00FA0008): {KEEP(*(.appDelay))}
.appKeyAddr LOAD(0x00FA000C): {KEEP(*(.appKeyAddr))}
} > word
GROUP :
{
.xptn_vectors (VLECODE) LOAD(0x011FF000): { }
.appKey LOAD(0x011FF110): {KEEP(*(.appKey))}
} > exception_handlers
Best regards,
Radu
Hi Radu,
After programming the rbf file to MCU, then reset the MCU ,it can't communicate with Rappid bootloader GUI.
But it can work without manual reset. which is not the same as you mentioned.
There is the other quesion. The application code can not work normally after the Rappid bootloader programs the MCU successfully.
Does the application code need to be allocated in a specific flash address?
Thanks a lot.
Best Regards,
Kent