Dear engineers,
I have a question. When I use the MPC5744P MBD toolbox, if I want to do a calibration test on freeMASTER, for example, I can read the freeMASTER input data and respond in the program. Is this feasible? What should I do if it is feasible? I did not find relevant information in the routine, thank you! ! !
Thanks with best regards,
Huang
Solved! Go to Solution.
Hi 260068845@qq.com,
Yes, that is perfectly feasible: you can use HTML and jscript to build such calibration test framework.
FYI, there is an MPC5744P FreeMASTER example and a short description in this article/video: https://community.nxp.com/thread/455228
A more detailed example can be found attached here but is made for S32K - anyhow the FreeMASTER is generic so you can reuse it as a source of inspiration: just check the bldc_closedloop_control.htm file
In regards with the data handling via HTML please check the chapter 6 in the pdf document attached.
Hope this helps - and we look forward to see a screenshot with your implementation
Best regards,
Daniel
Hi 260068845@qq.com,
Yes, that is perfectly feasible: you can use HTML and jscript to build such calibration test framework.
FYI, there is an MPC5744P FreeMASTER example and a short description in this article/video: https://community.nxp.com/thread/455228
A more detailed example can be found attached here but is made for S32K - anyhow the FreeMASTER is generic so you can reuse it as a source of inspiration: just check the bldc_closedloop_control.htm file
In regards with the data handling via HTML please check the chapter 6 in the pdf document attached.
Hope this helps - and we look forward to see a screenshot with your implementation
Best regards,
Daniel
It is possible to show it using an openloop control model or using a general model everybody can implement (without motor / closed loop).
It is helpful to check the operation of FREEMASTER and Simulink.
Thank you.I will try it.