PIL for MPC5744

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PIL for MPC5744

跳至解决方案
2,579 次查看
ykarata1
Contributor IV

Dear All,

I want to implement PIL for MPC5744 DEV_KIT and I have followed  PART 15: Processor-in-the-Loop (PIL) Validation video of NXP.

I could not operate the PIL system. I am getting MP57xx Config is missing error despite of model has it.

I have shared models at the attachment.

Any help will be appreciated.

标记 (1)
1 解答
2,522 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Unfortunately, because we are using a custom tlc file, running PIL requires inserting our config block in all the referenced models as well. This should not affect the simulation running for the referenced models. Once I've added the config block, the PIL ran.

pastedImage_1.png

Hope this helps,

Marius

在原帖中查看解决方案

3 回复数
2,523 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Unfortunately, because we are using a custom tlc file, running PIL requires inserting our config block in all the referenced models as well. This should not affect the simulation running for the referenced models. Once I've added the config block, the PIL ran.

pastedImage_1.png

Hope this helps,

Marius

2,523 次查看
ykarata1
Contributor IV

Dear mariuslucianandrei‌,

Thanks for your support at PIL sample.

When I increased complexity and size of the model , It seems that I get a communication error. I am using same config and same model parameters. What may be the problem?

How can I solve that?

Thanks.

Inside of model:

pastedImage_1.png

PIL_VERIFICATTION:

pastedImage_2.png

RESULT:

pastedImage_4.png

0 项奖励
回复
2,523 次查看
ykarata1
Contributor IV

Thank you very much mariuslucianandrei

I have added config file to the model and it has worked.

Thanks a lot. That was my first PIL experience. :smileygrin: